CANOPEN.MONITORSYNC

Description

Configures whether EtherCat/CANBus drives monitor PDO reception. The drive expects a synchronization event every CANOPEN.SAMPLEPERIOD once the first event is received. If three events are missed in a row, a fault is generated. Monitoring begins when this keyword is set and the first SYNC/PDO is received.

  • For EtherCAT, PDO reception is monitored.
  • For CANBus, SYNC messages are monitored.

Context

See EtherCAT and CANopen Overview.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

CANBus: 0 (Off)

EtherCAT: 1 (On)

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

CAN bus and EtherCATdrives: AKD2G-SPC and AKD2G-SPE

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CANOPEN.MONITORSYNC

300bh

01h

Unsigned8

-

-

Read/Write

No